Detected Internal Error Logs
Description
The last 20 detected internal errors are recorded by the LTMT main unit. Each detected internal error log is composed of 8 registers.
A read request of 8xn registers is necessary to read n detected internal error logs, where 8 is the number of registers for each detected internal error log.
The order and the description of the registers for detected internal error log 1 are valid for the other detected internal error logs.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
Description |
|---|---|---|
| 0x1F40–0x1F47 (8001–8008) |
82 : 79 : 01 – 82 : 79 : 08 |
Detected internal error log 1 (most recent log) |
| ... | ... | ... |
| 0x1F40–0x1F47 (8001+8x(n-1) – 8008+8x(n-1)) | ... | Detected internal error log n |
| ... | ... | ... |
| 0x1FD8–0x1FDF (8153–8160) |
82 : 8C : 01 – 82 : 8C : 08 |
Detected internal error log 20 |
Detected Internal Error Log 1 Registers
The table lists the registers for the detected internal error log 1.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X |
Unit |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|---|
|
0x1F40 (8001) |
82 : 79 : 01 |
R |
– |
– |
UINT16 |
Y | Date and time |
|
0x1F44 (8005) |
82 : 79 : 05 |
R |
– |
– |
UINT16 |
Y | Device internal error code |
|
0x1F45 (8006) |
82 : 79 : 06 |
R |
– |
– |
UINT16 |
Y | Reserved |