Maximum Number of Starts
The table lists the maximum number of starts for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0EB6 (3767) |
83 : 03 : 11 |
RW |
1 |
– |
UINT16 |
|
1 |
Y |
Function setting |
|
0x0EB7 (3768) |
83 : 03 : 12 |
RW |
1 |
– |
UINT16 |
1–30 |
6 |
Y |
Permissive starts |
|
0x0EB8 (3769) |
83 : 03 : 13 |
RW |
1 |
min |
UINT16 |
15–60 |
30 |
Y |
Reference time |
|
0x0EB9 (3770) |
83 : 03 : 14 |
RW |
1 |
min |
UINT16 |
1–120 |
5 |
Y |
Inhibit period |
|
0x0EBA (3771) |
83 : 03 : 15 |
RW |
1 |
min |
UINT16 |
0–120 |
0 |
Y |
Time between starts |
|
0x0EBB (3772) |
83 : 03 : 16 |
– |
– |
– |
– |
– |
– |
– |
Reserved |