DOCA0258EN-00

Modbus TCP Global Diagnostics

The table lists the Modbus TCP global diagnostics for the Modbus TCP/IP communication.

Modbus TCP/IP Address (Register)

RW

X Unit Range Default value

Svd

Description

0xA804 (43013)

R

1

0–1

Port Status

0xA805 (43014)

R

1

0–1

Open TCP Connection

0xA806 (43015)

R

1

0–4294967295

Total Received Messages

0xA8048 (43017)

R

1

0–4294967295

Total Transmitted Messages

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?