Stalled Rotor Protection
The table lists the stalled rotor protection for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0DBE (3519) |
83 : 01 : 13 |
RW |
1 |
– |
UINT16 |
|
2 |
Y |
Function setting |
|
0x0DBF (3520) |
83 : 01 : 14 |
RW |
1 |
%IFLC |
UINT16 |
50–1000 |
200 |
Y |
Pickup |
|
0x0DC0 (3521) |
83 : 01 : 15 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
20 |
Y |
Time delay |
|
0x0DC1 (3522) |
83 : 01 : 16 |
RW |
1 |
%IFLC |
UINT16 |
50–1000 |
200 |
Y |
Alarm level |
|
0x0DC2 (3523) |
83 : 01 : 17 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0DC3 (3524) |
83 : 01 : 18 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset Delay |