DOCA0258EN-00

HMI Communication Loss

The table lists the HMI communication loss for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0EDE (3807)

83 : 03 : 39

RW

1

UINT16

  • 0: Disable

  • 1: Trip

  • 2: Alarm+Trip

0

Y

Function setting

0x0EDF (3808)

83 : 03 : 3A

RW

0.1

s

UINT16

10

Y

Time delay

0x0EE0 (3809)

83 : 03 : 3B

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI

  • Bit 2: Communication

  • Bit 3: Auto

3

Y

Reset mode

0x0EE1 (3810)

83 : 03 : 3C

RW

0.1

s

UINT16

0

Y

Auto-Reset delay

0x0EE2 (3811)

83 : 03 : 3D

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?