DOCA0258EN-00

Voltage Page Body

The Voltage page contains the following sub-menus:

Level 1 Level 2 Parameter Name
Voltage* Under Voltage Trip Counter Under Voltage Trip Counter
Over Voltage Trip Counter Over Voltage Trip Counter
Voltage Phase Loss Trip Counter Voltage Phase Loss Trip Counter
Voltage Imbalance Trip Counter Voltage Imbalance Trip Counter
Voltage Phase Reversal Trip Counter Voltage Phase Reversal Trip Counter
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?