Short Time Overcurrent Protection
The table lists the short time overcurrent protection for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0DD9 (3546) |
83 : 01 : 2E |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
|
0x0DDA (3547) |
83 : 01 : 2F |
RW |
1 |
%IFLC |
UINT16 |
100–1000 |
100 |
Y |
Pickup |
|
0x0DDB (3548) |
83 : 01 : 30 |
RW |
0.01 |
s |
UINT16 |
5–1000 |
5 |
Y |
Time delay |
|
0x0DDC (3549) |
83 : 01 : 31 |
RW |
1 |
%IFLC |
UINT16 |
100–1000 |
100 |
Y |
Alarm level |
|
0x0DDD (3550) |
83 : 01 : 32 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0DDE (3551) |
83 : 01 : 33 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0DDF (3552) |
83 : 01 : 34 |
– |
– |
– |
– |
– |
– |
– |
Reserved |