Voltage Dip
The table lists the voltage dip for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
No. |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0EAD (3758) |
83 : 03 : 08 |
1 |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
|
0x0EAE (3759) |
83 : 03 : 09 |
1 |
1 |
%Vn |
UINT16 |
20–90 |
90 |
Y |
Voltage dip |
|
0x0EAF (3760) |
83 : 03 : 0A |
1 |
1 |
%Vn |
UINT16 |
20–95 |
95 |
Y |
Voltage restoration |
|
0x0EB0 (3761) |
83 : 03 : 0B |
1 |
1 |
s |
UINT16 |
0–9999 |
2 |
Y |
Voltage dip restart timeout |
|
0x0EB1 (3762) |
83 : 03 : 0C |
1 |
1 |
s |
UINT16 |
0–301 |
4 |
Y |
Delayed restart timeout |
|
0x0EB2 (3763) |
83 : 03 : 0D |
1 |
1 |
– |
UINT16 |
|
0 |
Y |
Bypass STOP DI |
|
0x0EB3 (3764) |
83 : 03 : 0E |
1 |
1 |
s |
UINT16 |
0–4 |
2 |
Y |
Immediate restart timeout |
|
0x0EB4 (3765) |
83 : 03 : 0F |
1 |
1 |
s |
UINT16 |
1–9999 |
10 |
Y |
Load shedding timeout |
|
0x0EB5 (3766) |
83 : 03 : 10 |
1 |
– |
– |
– |
– |
– |
– |
Reserved |