DOCA0258EN-00

Primary and Secondary NTP or SNTP Server Name

The table lists the Primary and Secondary NTP or SNTP server name for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X Unit

Type

Range Default value

Svd

Description

0x13DA (5083)

88 : 01 : D0

RW

1

N/A

UINT16

0–65535
(step 1)

1

Y

primary server name (NTP/SNTP)

0x13EA (5099)

88 : 01 : E0

RW

1

N/A

UINT16

0–65535
(step 1)

0

Y

Secondary server name (NTP/SNTP)

0x13FA (5115)

88 : 01 : F0

RW

1

N/A

UINT16

0: Obtain IP from DHCP/BOOTP

1: Manual

0

Y

DNS Enable Disable

0x13FB (5116)

88 : 01 : F1

RW

1

N/A

UINT16

-

169

Y

reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.