DOCA0258EN-00

Voltage Phase Reversal Protection

The table lists the voltage phase reversal protection for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0E44 (3653)

83 : 02 : 1C

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

2

Y

Function setting

0x0E45 (3654)

83 : 02 : 1D

RW

0.1

s

UINT16

1–60000
(step 1)

1

Y

Time delay

0x0E46 (3655)

83 : 02 : 1E

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0E47 (3656)

83 : 02 : 1F

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0E48 (3657)

83 : 02 : 20

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?