Voltage Phase Loss Protection
The table lists the voltage phase loss protection for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0E38 (3641) |
83 : 02 : 10 |
RW |
1 |
– |
UINT16 |
|
2 |
Y |
Function setting |
|
0x0E39 (3642) |
83 : 02 : 11 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
1 |
Y |
Time delay |
|
0x0E3A (3643) |
83 : 02 : 12 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0E3B (3644) |
83 : 02 : 13 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0E3C (3645) |
83 : 02 : 14 |
– |
– |
– |
– |
– |
– |
– |
Reserved |