DOCA0258EN-00

Over Frequency Protection

The table lists the over frequency protection for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0E50 (3665)

83 : 02 : 28

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

0

Y

Function setting

0x0E51 (3666)

83 : 02 : 29

RW

1

%F*

UINT16

100–110
(step 1)

105

Y

Pickup

0x0E52 (3667)

83 : 02 : 2A

RW

0.1

s

UINT16

1–60000
(step 1)

1

Y

Time delay

0x0E53 (3668)

83 : 02 : 2B

RW

1

%F*

UINT16

100–110
(step 1)

105

Y

Alarm level

0x0E54 (3669)

83 : 02 : 2C

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0E55 (3670)

83 : 02 : 2D

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0E56 (3671)

83 : 02 : 2E

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?