DOCA0258EN-00

Common Trip, Alarm, and Pickup Status

The table lists the common trip, alarm, and pickup status for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

RW

Type

Svd

Description

0x00E0 (225)

R

BOOL N

Pickup status

0x00E1 (226)

R

BOOL N

Alarm status

0x00E2 (227)

R

BOOL N

Trip status

0x00E3 (228)

R

BOOL N

Motor stop error detection trip

0x00E4 (229)

Reserved

0x00E5 (230)

R

BOOL N

Block output

0x00E6 (231)

R

BOOL N

Logic test interrupted trip

0x00E7 (232)

R

BOOL N

Logic test interrupted pickup

0x00E8 (233)

R

BOOL N

Stucked reset key trip

0x00E9–0x00EF (234–240)

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?