DOCA0258EN-00

Communication Configuration

The table lists the communication configuration for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X Unit

Type

Range Default value

Svd

Description

0x137B (4988)

88 : 01 : 71

RW

1

N/A

UINT16

0–255
(step 1)

192

Y

client IP Address - Byte 3

0x137C (4989)

88 : 01 : 72

RW

1

N/A

UINT16

0–255
(step 1)

168

Y

client IP Address - Byte 2

0x137D (4990)

88 : 01 : 73

RW

1

N/A

UINT16

0–255
(step 1)

1

Y

client IP Address - Byte 1

0x137E (4991)

88 : 01 : 74

RW

1

N/A

UINT16

0–255
(step 1)

100

Y

client IP Address - Byte 0

0x137F (4992)

88 : 01 : 75

RW

1

N/A

UINT16

0–100
(step 1)

2

Y

Communication timeout

0x1380 (4993)

88 : 01 : 76

RW

1

N/A

UINT16

0: Both Pri and Sec as Str name

1: Pri as IP and Sec as Str name

2: Pri as Str name and Sec as IP

3: Pri as IP and Sec as IP

0

Y

Numeric or String for NTP Primary and Secondary for internal Purpose

0x1381 (4994)

88 : 01 : 77

RW

1

N/A

UINT16

1–65535
(step 1)

502

Y

Modbus TCP port

0x1382 (4995)

88 : 01 : 78

RW

1

N/A

UINT16

0: Disable

1: Enable

0

Y

Broadcast Storm Protection Enable/Disable

0x1383 (4996)

88 : 01 : 79

RW

1

N/A

UINT16

0: lowest (Display Name and not rate)1000 packets/seconds

1: low: 2000 packets/seconds

2: Medium Low: 3000 packets/seconds

3: Medium High

4: High 5 - Highest

0

Y

Broadcast Storm Protection

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?