DOCA0258EN-00

Date Time Statistics

The table lists the date time statistics for the Modbus TCP/IP communication.

Modbus TCP/IP Address (Register)

RW

X Unit Range Default value

Svd

Description

0xA894 (43157)

R

1

0: Manual

1: NTP

2: FB

Time Source

0xA895 (43158)

R

1

0–1

Last Synchronized

0xA89B (43164)

R

1

0: Not synchronized

1: Synchronised

NTP Synchronization status

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?