Voltage Imbalance Protection
The table lists the voltage imbalance protection for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0E3D (3646) |
83 : 02 : 15 |
RW |
1 |
– |
UINT16 |
|
3 |
Y |
Function setting |
|
0x0E3E (3647) |
83 : 02 : 16 |
RW |
1 |
%Vn |
UINT16 |
5–50 |
10 |
Y |
Pickup |
|
0x0E3F (3648) |
83 : 02 : 17 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
100 |
Y |
Time delay |
|
0x0E40 (3649) |
83 : 02 : 18 |
RW |
1 |
– |
UINT16 |
5–50 |
10 |
N |
Alarm level |
|
0x0E41 (3650) |
83 : 02 : 19 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0E42 (3651) |
83 : 02 : 1A |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0E43 (3652) |
83 : 02 : 1B |
– |
– |
– |
– |
– |
– |
– |
Reserved |