DOCA0258EN-00

Custom Logic Input Status

The table lists the custom logic input status for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

RW

Type

Svd

Description

0x0040 (65)

R

BOOL

N

Local-START> DI
0x0041 (66)

R

BOOL

N

Local-STOP DI

0x0042 (67)

R

BOOL

N

Local-START>> DI

0x0043 (68)

R

BOOL

N

Mode selection 1

0x0044 (69)

R

BOOL

N

Local-START< DI

0x0045 (70)

R

BOOL

N

Local-START<< DI

0x0046 (71)

R

BOOL

N

Remote-START> DI

0x0047 (72)

R

BOOL

N

Remote-STOP DI

0x0048 (73)

R

BOOL

N

Remote-START>> DI

0x0049 (74)

R

BOOL

N

Mode selection 2

0x004A (75)

R

BOOL

N

Remote-START< DI

0x004B (76)

R

BOOL

N

Remote-START<< DI

0x004C (77)

R

BOOL

N

Run DI

0x004D (78)

R

BOOL

N

Speed change DI

0x004E–0x005F (79–96)

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?