DOCA0258EN-00

Standard Web Server User Interface

All web server pages share a consistent layout, with the window divided into three distinct sections.

Legend

Area

Description

A Menu

Banner displayed on every page, showing links to the menus:

  • Monitoring & Control

  • Diagnostics

  • Maintenance

  • Settings

  • Security

B Sub-menu treeview Links to the pages related to the selected menu. The treeview always displays the menu name in which the user is navigating
C Page body Information related to the contextual page selected in the menu or sub-menu
NOTE: Not all the parameters listed in the following pages will appear in the web server sub-menus. The parameters available depend on the LTMT main unit type and configuration of the TeSys Tera system.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?