DOCA0258EN-00

LLDP Data Table Object

Description

The LLDP data table object displays a record of all the adjacent LLDP implementing devices that are currently active according to the receive state machine of the LLDP protocol.

Class Code

The LLDP data table object class code is 0x10A.

Class Attributes

Attribute ID

Name

Access

Description

0x01

Revision

R

The LDP data table object implementation revision.

Returns 0x01.

0x02

Maximum Instance

R

Returns 0x01 to represent a single instance.

0x03

Number of Instances

R

The number of object instances.

Returns 0x01.

Class Services

Service Code

Name

Description

0x01

Get Attribute All

Returns the value of all class attributes.

0x0E

Get Attribute Single

Returns the value of the specified attribute.

0x11

Find Next Object Instance

Locate the next object instance, if any

Instance Attributes

Attribute ID

Name

Access

Description

0x01

Ethernet link instance number

R

Local instance number of the Ethernet link object that corresponds to the physical Ethernet port on which the LLDP frame for this instance was received, if known.

0x02

MAC address

R

Neighboring MAC address received from the CIP MAC address, chassis ID, or port ID TLV.

0x03

Interface label

R

Neighboring interface label received from the CIP Interface Label, Chassis ID, or Port ID TLV.

0x04

Time to live

R

Number of seconds the neighboring information is considered valid.

0x05

System capabilities TLV, system capabilities and enabled capabilities

R

Contain bitmaps representing the capabilities that define the primary function(s) of the neighboring system.

0x06

IPv4 management addresses: Management address count and management address

R

Contains neighboring device CIP.

0x07

CIP Identification: Vendor ID, device type, product code, major revision, minor revision and CIP serial number

R

Identification of CIP TLV of the neighboring device.

0x08

Additional Ethernet capabilities

R

TLV indicating Ethernet Preemption Support from the neighboring device.

0x09

Last change

R

Value of sysUpTime recorded the last time any attribute in this instance changed.

Instance Services

Service Code

Name

Description

0x01

Get Attribute All

Returns the value of all class attributes.

0x0E

Get Attribute Single

Returns the value of the specified attribute.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?