IP Network List Page Body
HTTPS Section
On the HTTP section, proceed as follows.
-
Enter the port number in the Port box.
NOTE: The default port number is 443. -
Confirm with APPLY.
Modbus TCP Section
On the Modbus TCP section, proceed as follows.
-
Use the toggle key to turn the Modbus TCP protocol on or off.
-
Enter the port number in the Port box.
NOTE: The default port number is 502. -
Confirm with APPLY.
Device Discovery Section
On the Device Discovery section, proceed as follows.
-
Use the toggle key to turn the Device Discovery feature on or off.
-
Use the toggle key to turn the Non Silent Mode feature on or off.
-
Enter the port number in the Port box.
NOTE: The default port number is 63. -
Confirm with APPLY.
DNS Section
On the DNS section, proceed as follows.
-
Enter the port number in the Port box.
NOTE: The default port number is 53. -
Confirm with APPLY.
Modbus RTU Section
On the Modbus RTU section, proceed as follows.
-
Use the toggle key to turn the Modbus RTU protocol on or off.
-
Confirm with APPLY.