DOCA0258EN-00

IP Filtering Global Access List

The table lists the IP Filtering Global Access for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X Unit

Type

Range Default value

Svd

Description

0x1385 (4998)

88 : 01 : 7B

RW

1

N/A

UINT16

0: None

1: Read/Write

0

Y

Access Level for first IP allow list

0x1386 (4999)

88 : 01 : 7C

RW

1

N/A

UINT16

0–255
(step 1)

0

Y

IP allowlist range1 address - Byte 3

0x1387 (5000)

88 : 01 : 7D

RW

1

N/A

UINT16

0–255
(step 1)

0

Y

IP allowlist range1 address - Byte 2

0x1388 (5001)

88 : 01 : 7E

RW

1

N/A

UINT16

0–255
(step 1)

0

Y

IP allowlist range1 address - Byte 1

0x1389 (5002)

88 : 01 : 7F

RW

1

N/A

UINT16

0–255
(step 1)

0

Y

IP allowlist range1 address - Byte 0

0x138A (5003)

88 : 01 : 80

RW

1

N/A

UINT16

0–255
(step 1)

0

Y

NTP/SNTP secondary server Byte 3

0x138B (5004)

88 : 01 : 81

RW

1

N/A

UINT16

0–255
(step 1)

0

Y

NTP/SNTP secondary server Byte 2

0x138C (5005)

88 : 01 : 82

RW

1

N/A

UINT16

0–255
(step 1)

0

Y

NTP/SNTP secondary server Byte 1

0x138D (5006)

88 : 01 : 83

RW

1

N/A

UINT16

0–255
(step 1)

0

Y

NTP/SNTP secondary server Byte 0

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?