DOCA0258EN-00

Overview

The IP Allow list page allows you to modify the IP address settings of the TeSys Tera system.

NOTE: The TeSys Tera system supports field bus communication only from IP addresses or ranges that are approved and have this function enabled.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?