DOCA0258EN-00

Analog Output Settings

The TeSys Tera system supports up to two analog outputs with two LTMTAN21 expansion modules.

The settings of each analog output are made up of five registers.

The characteristics (Range, Unit, and X) of the setting registers depend on the analog output source selected. Refer to Analog Output Source Settings.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

Type

Default value

Svd

Description

0x128E (4751)

86 : 03 : 01

RW

UINT16

0

Y

AO1 source

0x128F (4752)

86 : 03 : 02

Reserved

0x1290 (4753)

86 : 03 : 03

RW

UINT16

0

Y

AO1 source minimum range

0x1291 (4754)

86 : 03 : 04

Reserved

0x1292 (4755)

86 : 03 : 05

RW

UINT16

0

Y

AO1 source maximum range

0x1293–0x1298 (4756–4761)

86 : 03 : 06

Reserved

0x1299 (4762)

86 : 03 : 0C

RW

UINT16

0

Y

AO2 source

0x129A (4763)

86 : 03 : 0D

Reserved

0x129B (4764)

86 : 03 : 0E

RW

UINT16

0

Y

AO2 source minimum range

0x129C (4765)

86 : 03 : 0F

Reserved

0x129D (4766)

86 : 03 : 10

RW

UINT16

0

Y

AO2 source maximum range

0x129E–0x12A3 (4767–4772)

86 : 03 : 11

Reserved

Analog Output Source Settings

The table lists the minimum and maximum setting values for each analog output source.

Analog Output source

Value

AO source minimum range

AO source maximum range

X

Unit

None

0

L1 RMS current

1

10

1000

1

%FLC1

L2 RMS current

2

10

1000

1

%FLC1

L3 RMS current

3

10

1000

1

%FLC1

Average current

4

10

1000

1

%FLC1

L1-L2 RMS voltage

5

20

150

1

%Vn

L2-L3 RMS voltage

6

20

150

1

%Vn

L3-L1 RMS voltage

7

20

150

1

%Vn

Average voltage

8

20

150

1

%Vn

System frequency

9

50

150

1

%Fn

Total active power

10

20

1000

1

%Pn

Total apparent power   

11

20

1000

1

%Pn

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?