DOCA0258EN-00

Digital Input Settings

Description

The TeSys Tera system supports maximum 32 digital inputs:

  • Four digital inputs on the LTMT main unit.
  • Up to 28 digital inputs with LTMT expansion modules.

Each digital input setting is made up of three registers. The order and the description of the settings for digital input 1 are valid for the other digital inputs.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

No. Description DI location

0x1194 (4501)

86 : 01 : 01

3

Digital input 1 settings

DI1 on LTMT main unit

0x1197 (4504)

86 : 01 : 04

3

Digital input 2 settings

DI2 on LTMT main unit

0x119A (4507)

86 : 01 : 07

3

Digital input 3 settings

DI3 on LTMT main unit

0x119D (4510)

86 : 01 : 0A

3

Digital input 4 settings

DI4 on LTMT main unit

0x11A0 (4513)

86 : 01 : 0D

3

Digital input 5 settings

DI5 on LTMT expansion module

0x11A3 (4516)

86 : 01 : 10

3

Digital input 6 settings

DI6 on LTMT expansion module

0x11A6 (4519)

86 : 01 : 13

3

Digital input 7 settings

DI7 on LTMT expansion module

0x11A9 (4522)

86 : 01 : 16

3

Digital input 8 settings

DI8 on LTMT expansion module

0x11AC (4525)

86 : 01 : 19

3

Digital input 9 settings

DI9 on LTMT expansion module

0x11AF (4528)

86 : 01 : 1C

3

Digital input 10 settings

DI10 on LTMT expansion module

0x11B2 (4531)

86 : 01 : 1F

3

Digital input 11 settings

DI11 on LTMT expansion module

0x11B5 (4534)

86 : 01 : 22

3

Digital input 12 settings

DI12 on LTMT expansion module

0x11B8 (4537)

86 : 01 : 25

3

Digital input 13 settings

DI13 on LTMT expansion module

0x11BB (4540)

86 : 01 : 28

3

Digital input 14 settings

DI14 on LTMT expansion module

0x11BE (4543)

86 : 01 : 2B

3

Digital input 15 settings

DI15 on LTMT expansion module

0x11C1 (4546)

86 : 01 : 2E

3

Digital input 16 settings

DI16 on LTMT expansion module

0x11C4 (4549)

86 : 01 : 31

3

Digital input 17 settings

DI17 on LTMT expansion module

0x11C7 (4552)

86 : 01 : 34

3

Digital input 18 settings

DI18 on LTMT expansion module

0x11CA (4555)

86 : 01 : 37

3

Digital input 19 settings

DI19 on LTMT expansion module

0x11CD (4558)

86 : 01 : 3A

3

Digital input 20 settings

DI20 on LTMT expansion module

0x11D0 (4561)

86 : 01 : 3D

3

Digital input 21 settings

DI21 on LTMT expansion module

0x11D3 (4564)

86 : 01 : 40

3

Digital input 22 settings

DI22 on LTMT expansion module

0x11D6 (4567)

86 : 01 : 43

3

Digital input 23 settings

DI23 on LTMT expansion module

0x11D9 (4570)

86 : 01 : 46

3

Digital input 24 settings

DI24 on LTMT expansion module

0x11DC (4573)–0x11F1 (4594

86 : 01 : 49– 86 : 01 : 5E

Reserved

The settings of the four digital inputs on the LTMT main unit corresponds to the settings of digital input 1 to digital input 4.

The settings of digital inputs on a LTMT expansion module are defined according to the LTMT expansion module configuration.

Example:

If the TeSys Tera system is composed of:

  • One LTMT main unit.

  • One LTMTIN42BD expansion module or LTMTIN42FM expansion module with four digital inputs, configured as expansion module 1.

Then:

  • Digital input 1 settings to Digital input 4 settings are valid for DI1 to DI4 on the LTMT main unit.
  • Digital input 5 settings to Digital input 8 settings are valid for DI5 to DI8 on the LTMTIN42BD expansion module or LTMTIN42FM expansion module.

Digital Input 1 Settings

The table lists the registers for the digital input settings.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X Unit

Type

Range Default value

Svd

Description

0x1194 (4501)

86 : 01 : 01

RW

1

UINT16

0: Active high

1: Active low

0

Y

Digital input 1 trigger type

0x1195 (4502)

86 : 01 : 02

RW

1

UINT16

0–38
(step 1)

4

Y

DI Input Source
0x1196 (4503)

86 : 01 : 03

RW

1 ms UINT16

0–60000
(step 10)

10

Y

Digital input 1 validation time

DI Input Source

The table lists the input source for the digital input settings.

Register value DI input source

0

Other

1

Trip Reset DI

2

Breaker Close DI

3

Breaker Open DI

4

Local-START> DI

5

Local-START>> DI

6

Local-STOP DI

7

Local-START< DI

8

Local-START<< DI

9

Remote-START> DI

10

Remote-START>> DI

11

Remote-STOP DI

12

Remote-START< DI

13

Remote-START<< DI

14

Interlock 1

15

Interlock 2

16

Interlock 3

17

Interlock 4

18

Interlock 5

19

Interlock 6

20

Interlock 7

21

Interlock 8

22

Interlock 9

23

Interlock 10

24

Interlock 11

25

Interlock 12

26

Contactor Open DI

27

Run DI

28

Block Input

29

Logic Test DI

30

Mode Selection 1

31

Mode Selection 2

32

Speed Change

33

Forced Start

34

Forced Stop

35

Self Test without Trip

36

Self Test with Trip

37

Soft Starter Reset DI

38

None

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?