DOCA0258EN-00

Overview

The Diagnostics page displays the motor status, alarm or trip status, logs, device internal status, communication status, trip counters, and device information of the TeSys Tera system.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?