DOCA0258EN-00

Field Bus Protocol Page Body

The Field Bus Protocol page contains the following sub-menus:

Level 1 Level 2 Parameter Name
Field Bus Protocol Protocol selection Protocol selection. Possible values:
  • Modbus TCP

  • EtherNet/IP
Communication Loss Timeout Communication Loss Timeout
Client IP address Client IP address
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?