DOCA0258EN-00

IO Details Page Body

The IO Details page contains the following sub-menus:

Level 1 Level 2 Level 3 Parameter Name
Main Module Digital IO Digital Input 1 Digital Input 1
Digital Input 2 Digital Input 2
Digital Input 3 Digital Input 3
Digital Input 4 Digital Input 4
Digital Output 1 Digital Output 1
Digital Output 2 Digital Output 2
Digital Output 3 Digital Output 3
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?