IP Filtering Exceptional List
The table lists the IP Filtering Exceptional List for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X | Unit |
Type |
Range | Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x138E (5007) |
88 : 01 : 84 |
RW |
1 |
N/A |
UINT16 |
1: None 1: Read/Write |
0 |
Y |
Access Level for first IP |
|
0x138F (5008) |
88 : 01 : 85 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range1 address - Byte 3 |
|
0x1390 (5009) |
88 : 01 : 86 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range1 address - Byte 2 |
|
0x1391 (5010) |
88 : 01 : 87 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range1 address - Byte 1 |
|
0x1392 (5011) |
88 : 01 : 88 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range1 address - Byte 0 |
|
0x1393 (5012) |
88 : 01 : 89 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
DNS Primary Server address Byte 3 |
|
0x1394 (5013) |
88 : 01 : 8A |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
DNS Primary Server address Byte 2 |
|
0x1395 (5014) |
88 : 01 : 8B |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
DNS Primary Server address Byte 1 |
|
0x1396 (5015) |
88 : 01 : 8C |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
DNS Primary Server address Byte 0 |
|
0x1397 (5016) |
88 : 01 : 8D |
RW |
1 |
N/A |
UINT16 |
1: None 1: Read/Write |
0 |
Y |
Access Level for second IP |
|
0x1398 (5017) |
88 : 01 : 8E |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range3 address - Byte 3 |
|
0x1399 (5018) |
88 : 01 : 8F |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range3 address - Byte 2 |
|
0x139A (5019) |
88 : 01 : 90 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range3 address - Byte 1 |
|
0x139B (5020) |
88 : 01 : 91 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range3 address - Byte 0 |
|
0x139C (5021) |
88 : 01 : 92 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
DNS Secondary Server address Byte 3 |
|
0x139D (5022) |
88 : 01 : 93 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
DNS Secondary Server address Byte 2 |
|
0x139E (5023) |
88 : 01 : 94 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
DNS Secondary Server address Byte 1 |
|
0x139F (5024) |
88 : 01 : 95 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
DNS Secondary Server address Byte 0 |
|
0x13A0 (5025) |
88 : 01 : 96 |
RW |
1 |
N/A |
UINT16 |
1: None 1: Read/Write |
0 |
Y |
Access Level for fourth IP |
|
0x13A1 (5026) |
88 : 01 : 97 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range4 address - Byte 3 |
|
0x13A2 (5027) |
88 : 01 : 98 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range4 address - Byte 2 |
|
0x13A3 (5028) |
88 : 01 : 99 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range4 address - Byte 1 |
|
0x13A4 (5029) |
88 : 01 : 9A |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range4 address - Byte 0 |
|
0x13A5 (5030) |
88 : 01 : 9B |
RW |
1 |
N/A |
UINT16 |
- |
0 |
Y |
reserved |
|
0x13A6 (5031) |
88 : 01 : 9C |
RW |
1 |
N/A |
UINT16 |
- |
0 |
Y |
reserved |
|
0x13A7 (5032) |
88 : 01 : 9D |
RW |
1 |
N/A |
UINT16 |
- |
0 |
Y |
reserved |
|
0x13A8 (5033) |
88 : 01 : 9E |
RW |
1 |
N/A |
UINT16 |
- |
0 |
Y |
reserved |
|
0x13A9 (5034) |
88 : 01 : 9F |
RW |
1 |
N/A |
UINT16 |
1: None 1: Read/Write |
0 |
Y |
Access Level for fourth IP |
|
0x13AA (5035) |
88 : 01 : A0 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range5 address - Byte 3 |
|
0x13AB (5036) |
88 : 01 : A1 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range5 address - Byte 2 |
|
0x13AC (5037) |
88 : 01 : A2 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range5 address - Byte 1 |
|
0x13AD (5038) |
88 : 01 : A3 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range5 address - Byte 0 |
|
0x13AE (5039) |
88 : 01 : A4 |
RW |
1 |
N/A |
UINT16 |
- |
0 |
Y |
reserved |
|
0x13AF (5040) |
88 : 01 : A5 |
RW |
1 |
N/A |
UINT16 |
- |
0 |
Y |
reserved |
|
0x13B0 (5041) |
88 : 01 : A6 |
RW |
1 |
N/A |
UINT16 |
- |
0 |
Y |
reserved |
|
0x13B1 (5042) |
88 : 01 : A7 |
RW |
1 |
N/A |
UINT16 |
- |
0 |
Y |
reserved |
|
0x13B2 (5043) |
88 : 01 : A8 |
RW |
1 |
N/A |
UINT16 |
1: None 1: Read/Write |
0 |
Y |
Access Level for fifth IP |
|
0x13B3 (5044) |
88 : 01 : A9 |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range5 address - Byte 3 |
|
0x13B4 (5045) |
88 : 01 : AA |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range5 address - Byte 2 |
|
0x13B5 (5046) |
88 : 01 : AB |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range5 address - Byte 1 |
|
0x13B6 (5047) |
88 : 01 : AC |
RW |
1 |
N/A |
UINT16 |
0–255 (step 1) |
0 |
Y |
IP allowlist range5 address - Byte 0 |
|
0x13B7 (5048) |
88 : 01 : AD |
RW |
1 |
N/A |
UINT16 |
- |
0 |
Y |
reserved |
|
0x13B8 (5049) |
88 : 01 : AE |
RW |
1 |
N/A |
UINT16 |
- |
0 |
Y |
reserved |
|
0x13B9 (5050) |
88 : 01 : AF |
RW |
1 |
N/A |
UINT16 |
- |
0 |
Y |
reserved |
|
0x13BA (5051) |
88 : 01 : B0 |
RW |
1 |
N/A |
UINT16 |
- |
0 |
Y |
reserved |