DOCA0258EN-00

Event Logs

Description

The last 100 events are recorded by the LTMT main unit. Each event log is composed of 8 registers.

A read request of 8xn registers is necessary to read n event logs, where 8 is the number of registers for each event log.

The order and the description of the registers for event log 1 are valid for the other event logs.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

Description
0x1B58–0x1B5F (7001–7008)

82 : 15 : 01 – 82 : 15 : 08

Event log 1 (most recent log)
... ... ...
0x1858–0x1B57 (7001+8x(n-1) – 7008+8x(n-1)) ... Event log n
... ... ...
0x1E70–0x1E77 (7793–7800)

82 : 114 : 01 – 82 : 114 : 08

Event log 100

Event Log 1 Registers

The table lists the registers for the event log 1.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X

Unit

Type

Svd

Description

0x1B58 (7001)

82 : 15 : 01

R

UINT16

Y

Date and Time

0x1B5C

82 : 15 : 05

R

UINT16

Y

Event code

0x1B5D

82 : 15 : 06

R

UINT16

Y Reserved
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?