DOCA0258EN-00

Protection Function Status

Protection Alarm Status

The table lists the protection alarm status for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

RW

Type

Svd

Description

0x0100 (257)

R

BOOL N

Thermal overload alarm

0x0101 (258)

R

BOOL N

Locked rotor alarm

0x0102 (259)

R

BOOL N Stalled rotor alarm

0x0103 (260)

R

BOOL N

Definite time overcurrent alarm

0x0104 (261)

R

BOOL N

Normal inverse overcurrent alarm

0x0105 (262)

R

BOOL N

Short time overcurrent alarm

0x0106 (263)

R

BOOL N

Calculated ground current alarm

0x0107 (264)

R

BOOL N

Measured ground current alarm

0x0108 (265)

R

BOOL N

Phase under current alarm

0x0109 (266)

R

BOOL N

Current imbalance alarm

0x010A (267)

R

BOOL N

Current phase loss alarm

0x010B (268)

R

BOOL N

Current phase reversal alarm

0x010C (269)

R

BOOL N

Phase under voltage alarm

0x010D (270)

R

BOOL N

Phase over voltage alarm

0x010E (271)

R

BOOL N

Voltage phase loss alarm

0x010F (272)

R

BOOL N

Voltage imbalance alarm

0x0110 (273)

R

BOOL N

Voltage phase reversal alarm

0x0111 (274)

R

BOOL N

Under frequency alarm

0x0112 (275)

R

BOOL N

Over frequency alarm

0x0113 (276)

R

BOOL N

Reserved

0x0114 (277)

R

BOOL N

Communication loss alarm

0x0115 (278)

R

BOOL N

Over temperature alarm

0x0116 (279)

R

BOOL N

Under power alarm

0x0117 (280)

R

BOOL N

Over power alarm

0x0118 (281)

R

BOOL N

Under power factor alarm

0x0119–0x011A (282–283)

Reserved

0x011B (284)

R

BOOL N

HMI communication loss alarm

0x011C–0x011F (285–288)

Reserved

Protection Pickup Status

The table lists the protection pickup status for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

RW

Type

Svd

Description

0x0120 (289)

R

BOOL N

Thermal overload pickup

0x0121 (290)

R

BOOL N

Locked rotor pickup

0x0122 (291)

R

BOOL N

Stalled rotor pickup

0x0123 (292)

R

BOOL N

Definite time overcurrent pickup

0x0124 (293)

R

BOOL N

Normal inverse overcurrent pickup

0x0125 (294)

R

BOOL N

Short time overcurrent pickup

0x0126 (295)

R

BOOL N

Calculated ground current pickup

0x0127 (296)

R

BOOL N

Measured ground current pickup

0x0128 (297)

R

BOOL N

Phase under current pickup

0x0129 (298)

R

BOOL N

Current imbalance pickup

0x012A (299)

R

BOOL N

Current phase loss pickup

0x012B (300)

R

BOOL N

Current phase reversal pickup

0x012C (301)

R

BOOL N

Phase under voltage pickup

0x012D (302)

R

BOOL N

Phase over voltage pickup

0x012E (303)

R

BOOL N

Voltage phase loss pickup

0x012F (304)

R

BOOL N

Voltage imbalance pickup

0x0130 (305)

R

BOOL N

Voltage phase reversal pickup

0x0131 (306)

R

BOOL N

Under frequency pickup

0x0132 (307)

R

BOOL N

Over frequency pickup

0x0133 (308)

R

BOOL N

Excessive start time pickup

0x0134 (309)

R

BOOL N

Communication loss pickup

0x0135 (310)

R

BOOL N

Over temperature pickup

0x0136 (311)

R

BOOL N

Under power pickup

0x0137 (312)

R

BOOL N

Over power pickup

0x0138 (313)

R

BOOL N

Under power factor pickup

0x0139 (314)

Reserved

0x013A (315)

R

BOOL N

ICM pickup

0x013B (316)

R

BOOL N

HMI communication loss pickup

0x013C–0x013F (317–320)

Reserved

Protection Trip Status

The table lists the protection trip status for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

RW

Type

Svd

Description

0x0140 (321)

R

BOOL N

Thermal overload trip

0x0141 (322)

R

BOOL N

Locked rotor trip

0x0142 (323)

R

BOOL N

Stalled rotor trip

0x0143 (324)

R

BOOL N

Definite time overcurrent trip

0x0144 (325)

R

BOOL N

Normal inverse overcurrent trip

0x0145 (326)

R

BOOL N

Short time overcurrent trip

0x0146 (327)

R

BOOL N

Calculated ground current trip

0x0147 (328)

R

BOOL N

Measured ground current trip

0x0148 (329)

R

BOOL N

Phase under current trip

0x0149 (330)

R

BOOL N

Current imbalance trip

0x014A (331)

R

BOOL N

Current phase loss trip

0x014B (332)

R

BOOL N

Current phase reversal trip

0x014C (333)

R

BOOL N

Phase under voltage trip

0x014D (334)

R

BOOL N

Phase over voltage trip

0x014E (335)

R

BOOL N

Voltage phase loss trip

0x014F (336)

R

BOOL N

Voltage imbalance trip

0x0150 (337)

R

BOOL N

Voltage phase reversal trip

0x0151 (338)

R

BOOL N

Under frequency trip

0x0152 (339)

R

BOOL N

Over frequency trip

0x0153 (340)

R

BOOL N

Excessive start time trip

0x0154 (341)

R

BOOL N

Communication loss trip

0x0155 (342)

R

BOOL N

Over temperature trip

0x0156 (343)

R

BOOL N

Under power trip

0x0157 (344)

R

BOOL N

Over power trip

0x0158 (345)

R

BOOL N

Under power factor trip

0x0159 (346)

Reserved

0x015A (347)

R

BOOL N

ICM trip

0x015B (348)

R

BOOL N

HMI communication loss trip

0x015C–0x015F (349–352)

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?