DOCA0258EN-00

Internal LTMTCT/LTMTCTV Sensor Module Device Internal Error Detection Setting

The table lists the different device Internal error detection setting for the LTMTCT/LTMTCTV sensor module.

Modbus TCP/IP Address (Register)

RW

Type

Svd

Description

0x0280 (641)

R

BOOL N

Watchdog timeout detected

0x0281 (642)

R

BOOL N

ADC conversion error detected

0x0282 (643)

R

BOOL N

Flash error detected

0x0283 (644)

R

BOOL N

UART error detected

0x0284 (645)

R

BOOL N

Voltage configuration not detected

0x0285 (646)

Reserved

0x0286 (647)

R

BOOL N

Calibration error detected

0x0287 (648)

R

BOOL N

VL1 measurement error detected

0x0288 (649)

R

BOOL N

VL2 measurement error detected

0x0289 (650)

R

BOOL N

VL3 measurement error detected

0x028A (651)

R

BOOL N

IL1 low gain measurement error detected

0x028B (652)

R

BOOL N

IL1 high gain measurement error detected

0x028C (653)

R

BOOL N

IL2 low gain measurement error detected

0x028D (654)

R

BOOL N

IL2 high gain measurement error detected

0x028E (655)

R

BOOL N

IL3 low gain measurement error detected

0x028F (656)

R

BOOL N

IL3 high gain measurement error detected

0x0290–0x029F (657–672)

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?