DOCA0258EN-00

Product Versions

The hardware versions of the TeSys Tera system are coded XXYY in UINT32 registers, with the following format:

  • Register 0: Reserved

  • Register 1:

    • XXYY: Hexa code of ASCII characters

Example: the LTMT main unit hardware version A is coded:

  • Register 9163 = 0x0000

  • Register 9164 = 0x0041

The firmware versions of the TeSys Tera system are coded aaa.bbb.ccc in UINT32 registers, with the following format:

  • Register 0: ccc, revision

  • Register 1:

    • MSB: aaa, major version

    • LSB: bbb, minor version

Example: the LTMT main unit firmware version 001.002.004 is coded:

  • Register 9165 = 0x0004

  • Register 9166 = 0x0102

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

Type

Svd

Description

0x23CA (9163)

73 : 01 : 0C

R

UINT32

Y

LTMT main unit hardware version

0x23CC (9165)

73 : 01 : 0D

R

UINT32

Y

LTMT main unit firmware version

0x23CE (9167)

73 : 01 : 0E

R

UINT32

Y

LTMT main unit boot firmware version

0x23D0 (9169)

73 : 01 : 0F

R

UINT32

Y

LTMTCT/LTMTCTV sensor module hardware version

0x23D2 (9171)

73 : 01 : 10

R

UINT32

Y

LTMTCT/LTMTCTV sensor module firmware version

0x23D4 (9173)

73 : 01 : 11

R

UINT32

Y

LTMTCT/LTMTCTV sensor module boot firmware version

0x23D6 (9175)

73 : 01 : 12

R

UINT32

Y

LTMTCUF control operator unit hardware version

0x23D8 (9177)

73 : 01 : 13

R

UINT32

Y

LTMTCUF control operator unit firmware version

0x23DA (9179)

73 : 01 : 14

R

UINT32

Y

LTMTCUF control operator unit boot firmware version

0x23DC (9181)

73 : 01 : 15

R

UINT32

Y

LTMT expansion module 1 hardware version

0x23DE (9183)

73 : 01 : 16

R

UINT32

Y

LTMT expansion module 1 firmware version

0x23E0 (9185)

73 : 01 : 17

R

UINT32

Y

LTMT expansion module 1 boot firmware version

0x23E2 (9187)

73 : 01 : 18

R

UINT32

Y

LTMT expansion module 2 hardware version

0x23E4 (9189)

73 : 01 : 19

R

UINT32

Y

LTMT expansion module 2 firmware version

0x23E6 (9191)

73 : 01 : 1A

R

UINT32

Y

LTMT expansion module 2 boot firmware version

0x23E8 (9193)

73 : 01 : 1B

R

UINT32

Y

LTMT expansion module 3 hardware version

0x23EA (9195)

73 : 01 : 1C

R

UINT32

Y

LTMT expansion module 3 firmware version

0x23EC (9197)

73 : 01 : 1D

R

UINT32

Y

LTMT expansion module 3 boot firmware version

0x23EE (9199)

73 : 01 : 1E

R

UINT32

Y

LTMT expansion module 4 hardware version

0x23F0 (9201)

73 : 01 : 1F

R

UINT32

Y

LTMT expansion module 4 firmware version

0x23F2 (9203)

73 : 01 : 20

R

UINT32

Y

LTMT expansion module 4 boot firmware version

0x23F4 (9205)

73 : 01 : 21

R

UINT32

Y

LTMT expansion module 5 hardware version

0x23F6 (9207)

73 : 01 : 22

R

UINT32

Y

LTMT expansion module 5 firmware version

0x23F8 (9209)

73 : 01 : 23

R

UINT32

Y

LTMT expansion module 5 boot firmware version

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?