Trip Logs
Description
The last 20 encountered trips are recorded by the LTMT main unit. Each trip log is composed of 32 registers.
A read request of 32xn registers is necessary to read the last n trip logs, where 32 is the number of registers for each trip log.
The order and the description of the registers for trip log 1 are valid for the other trip logs.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
Description |
|---|---|---|
|
0x1770 (6001–6032) |
82 : 01: 01 – 82 : 01 : 32 |
Trip log 1 (most recent log) |
|
0x1790 (6033–6064) |
82 : 02 : 01 – 82 : 02 : 32 |
Trip log 2 |
|
0x17B0 (6065–6096) |
82 : 03: 01 – 82 : 03 : 32 |
Trip log 3 |
|
0x17D0 (6097–6128) |
82 : 04: 01 – 82 : 04 : 32 |
Trip log 4 |
|
0x17F0 (6129–6160) |
82 : 05: 01 – 82 : 05 : 32 |
Trip log 5 |
|
0x1810 (6161–6192) |
82 : 06: 01 – 82 : 06 : 32 |
Trip log 6 |
|
0x1830 (6193–6224) |
82 : 07: 01 – 82 : 07 : 32 |
Trip log 7 |
|
0x1850 (6225–6256) |
82 : 08: 01 – 82 : 08 : 32 |
Trip log 8 |
|
0x1870 (6257–6288) |
82 : 09: 01 – 82 : 09 : 32 |
Trip log 9 |
|
0x1890 6289–6320() |
82 : 10 : 01 – 82 : 10 : 32 |
Trip log 10 |
|
0x18B0 (6321–6352) |
82 : 11: 01 – 82 : 11 : 32 |
Trip log 11 |
|
0x18D0 (6353–6384) |
82 : 12 : 01 – 82 : 12 : 32 |
Trip log 12 |
|
0x18F0 (6385–6416) |
82 : 13 : 01 – 82 : 13 : 32 |
Trip log 13 |
|
0x1910 (6417–6448) |
82 : 14 : 01 – 82 : 14 : 32 |
Trip log 14 |
|
0x1930 (6449–6480) |
82 : 15 : 01 – 82 : 15 : 32 |
Trip log 15 |
|
0x1950 (6481–6512) |
82 : 16 : 01 – 82 : 16 : 32 |
Trip log 16 |
|
0x1970 (6513–6544) |
82 : 17 : 01 – 82 : 17 : 32 |
Trip log 17 |
|
0x1990 (6545–6576) |
82 : 18 : 01 – 82 : 18 : 32 |
Trip log 18 |
|
0x19B0 (6577–6608) |
82 : 19 : 01 – 82 : 19 : 32 |
Trip log 19 |
|
0x19D0 (6609–6640) |
82 : 20 : 01 – 82 : 21 : 32 |
Trip log 20 |
Trip Log 1 Registers
The table lists the registers for the trip log 1.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X |
Unit |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|---|
|
0x1770 (6001) |
82 : 01: 01 |
R |
– |
– |
UINT16 |
Y |
|
|
0x1774 (6005) |
82 : 01: 02 |
R |
– |
– |
UINT16 |
Y |
|
|
0x1775 (6006) |
82 : 01: 03 |
R |
1 |
% |
UINT16 |
Y |
Thermal memory |
|
0x1776 (6007) |
82 : 01: 04 |
R |
0.001 |
A |
UINT32 |
Y |
L1 RMS current |
|
0x1778 (6009) |
82 : 01: 05 |
R |
0.001 |
A |
UINT32 |
Y |
L2 RMS current |
|
0x177A (6011) |
82 : 01: 06 |
R |
0.001 |
A |
UINT32 |
Y |
L3 RMS current |
|
0x177C (6013) |
82 : 01: 07 |
R |
0.001 |
A |
UINT32 |
Y |
Calculated ground current |
|
0x177E (6015) |
82 : 01: 08 |
R |
0.001 |
A |
UINT32 |
Y |
Measured ground current |
|
0x1780 (6017) |
82 : 01: 09 |
R |
0.01 |
% |
UINT16 |
Y |
Current imbalance |
|
0x1781 (6018) |
82 : 01: 10 |
R |
1 |
– |
UINT16 |
Y |
Current phase sequence |
|
0x1782 (6019) |
82 : 01: 11 |
R |
0.1 |
V |
UINT16 |
Y |
L1-L2 RMS voltage |
|
0x1783 (6020) |
82 : 01: 12 |
R |
0.1 |
V |
UINT16 |
Y |
L2-L3 RMS voltage |
|
0x1784 (6021) |
82 : 01: 13 |
R |
0.1 |
V |
UINT16 |
Y |
L3-L1 RMS voltage |
|
0x1785 (6022) |
82 : 01: 14 |
R |
0.01 |
% |
UINT16 |
Y |
Voltage imbalance |
|
0x1787 (6023) |
82 : 01: 15 |
R |
1 |
– |
UINT16 |
Y |
Voltage phase sequence |
|
0x1787 (6024) |
82 : 01: 16 |
R |
0.01 |
Hz |
UINT16 |
Y |
System frequency |
|
0x1788 (6025) |
82 : 01: 17 |
R |
– |
– |
UINT16 |
Y |
MSB: System PF LSB: Motor status |
|
0x1789 (6026) |
82 : 01: 18 |
R |
0.1 |
– |
UINT16 |
Y |
MSB: L1 current THD LSB: L2 current THD |
|
0x178A (6027) |
82 : 01: 19 |
R |
0.1 |
– |
UINT16 |
Y |
MSB: L3 current THD LSB: L1 voltage THD |
|
0x178B (6028) |
82 : 01: 20 |
R |
0.1 |
– |
UINT16 |
Y |
MSB: L2 voltage THD LSB: L3 voltage THD |
|
0x178C (6029) |
82 : 01: 21 |
R |
0.001 |
– |
UINT32 |
Y |
Total active power |
|
0x178E (6031) |
82 : 01: 22 |
– |
– |
– |
– |
– |
Reserved |