Current Imbalance Protection
The table lists the current imbalance protection for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0DF6 (3575) |
83 : 01 : 4B |
RW |
1 |
– |
UINT16 |
|
3 |
Y |
Function setting |
|
0x0DF7 (3576) |
83 : 01 : 4C |
RW |
1 |
% |
UINT16 |
5–100 |
20 |
Y |
Pickup |
|
0x0DF8 (3577) |
83 : 01 : 4D |
RW |
0.1 |
s |
UINT16 |
1–60000 |
50 |
Y |
Time delay |
|
0x0DF9 (3578) |
83 : 01 : 4E |
RW |
1 |
– |
UINT16 |
5–100 |
20 |
Y |
Alarm level |
|
0x0DFA (3579) |
83 : 01 : 4F |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0DFB (3580) |
83 : 01 : 50 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0DFC (3581) |
83 : 01 : 51 |
– |
– |
– |
– |
– |
– |
– |
Reserved |