Calculated Ground Trip
The table lists the calculated ground trip for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0DE0 (3553) |
83 : 01 : 35 |
RW |
1 |
– |
UINT16 |
|
2 |
Y |
Function setting |
|
0x0DE1 (3554) |
83 : 01 : 36 |
RW |
1 |
%IFLC |
UINT16 |
10–500 |
20 |
Y |
Pickup |
|
0x0DE2 (3555) |
83 : 01 : 37 |
RW |
0.10 |
s |
UINT16 |
5–60000 |
20 |
Y |
Time delay |
|
0x0DE3 (3556) |
83 : 01 : 38 |
RW |
1 |
%IFLC |
UINT16 |
10–500 |
20 |
Y |
Alarm level |
|
0x0DE4 (3557) |
83 : 01 : 39 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0DE5 (3558) |
83 : 01 : 3A |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0DE6 (3559) |
83 : 01 : 3B |
RW |
1 |
– |
UINT16 |
|
0 |
N |
Function while motor starting |