DOCA0258EN-00

Motor Page Body

The Motor page contains the following sub-menus:

Level 1 Level 2 Parameter Name
Motor* Thermal Overload trip counter Thermal Overload trip counter
Locked rotor trip counter Locked rotor trip counter
Stalled rotor trip counter Stalled rotor trip counter
Excessive start time trip counter Excessive start time trip counter
Motor stop error detection trip counter Motor stop error detection trip counter
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?