DOCA0258EN-00

Analog Page Body

The Analog page contains the following sub-menus:

Level 1 Level 2 Parameter Name
Analog* Analog input 1 trip counter Analog input trip counter
Analog input 2 trip counter Analog input trip counter
Analog input 3 trip counter Analog input trip counter
Analog input 4 trip counter Analog input trip counter
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?