Command Data
The table lists the command data for Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
Type |
Svd |
Description |
|---|---|---|---|---|---|
|
0x02BC (701) |
6C : 01 : 01 |
RW |
BITMAP |
N |
Permissive command data
|
|
0x02BD–0x02BF (702–704) |
6C : 01 : 02 – 6C : 01 : 04 |
– |
– |
– |
Reserved |
|
0x02C0 (705) |
6C : 01 : 05 |
RW |
BITMAP |
N |
Command data 1
|
|
0x02C1 (706) |
6C : 01 : 06 |
RW |
BITMAP |
N |
Command
data 2
|