DOCA0258EN-00

Digital Output Status

The table lists the digital output status for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

RW

Type

Svd

Description

0x0020 (33)

R

BOOL

N

Digital output 1 

0x0021 (34)

R

BOOL

N

Digital output 2

0x0022 (35)

R

BOOL

N

Digital output 3

0x0023 (36)

R

BOOL

N

Digital output 4

0x0024 (37)

R

BOOL

N

Digital output 5

0x0025 (38)

R

BOOL

N

Digital output 6

0x0026 (39)

R

BOOL

N

Digital output 7

0x0027 (40)

R

BOOL

N

Digital output 8

0x0028 (41)

R

BOOL

N

Digital output 9

0x0029 (42)

R

BOOL

N

Digital output 10

0x002A (43)

R

BOOL

N

Digital output 11

0x002B (44)

R

BOOL

N

Digital output 12

0x002C (45)

R

BOOL

N

Digital output 13

0x002D–0x003F (46–64)

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?