DOCA0258EN-00

Digital Input Status

The table lists the digital input status for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

RW

Type

Svd

Description

0x0000 (1)

R

BOOL

N

Digital input 1 

0x0001 (2)

R

BOOL

N

Digital input 2

0x0002 (3)

R

BOOL

N

Digital input 3

0x0003 (4)

R

BOOL

N

Digital input 4

0x0004 (5)

R

BOOL

N

Digital input 5

0x0005 (6)

R

BOOL

N

Digital input 6

0x0006 (7)

R

BOOL

N

Digital input 7

0x0007 (8)

R

BOOL

N

Digital input 8

0x0008 (9)

R

BOOL

N

Digital input 9

0x0009 (10)

R

BOOL

N

Digital input 10

0x000A (11)

R

BOOL

N

Digital input 11

0x000B (12)

R

BOOL

N

Digital input 12

0x000C (13)

R

BOOL

N

Digital input 13

0x000D (14)

R

BOOL

N

Digital input 14

0x000E (15)

R

BOOL

N

Digital input 15

0x000F (16)

R

BOOL

N

Digital input 16

0x0010 (17)

R

BOOL

N

Digital input 17

0x0011 (18)

R

BOOL

N

Digital input 18

0x0012 (18)

R

BOOL

N

Digital input 19

0x0013 (19)

R

BOOL

N

Digital input 20

0x0014 (20)

R

BOOL

N

Digital input 21

0x0015 (21)

R

BOOL

N

Digital input 22

0x0016 (22)

R

BOOL

N

Digital input 23

0x0017 (23)

R

BOOL

N

Digital input 24

0x0018 (24)–0x001F (31)

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?