Port 2 Statistics
The table lists the port 2 statistic for the Modbus TCP/IP communication.
|
Modbus TCP/IP Address (Register) |
RW |
X | Unit | Range | Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|
|
0xA802 (43011) |
R |
1 | – |
0: 100 Mbps 1: 10 Mbps 2: Auto Negotiation 3: NA |
0 |
– |
Link Speed |
|
0xA803 (43012) |
R |
1 | – |
0: Full Duplex 1: Half Duplex 2: Auto Negotiation 3: NA |
0 |
– |
Duplex |