Hysteresis Settings
The table lists the registers for the hysteresis settings.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x109A (4251) |
84 : 04 : 01 |
RW |
1 |
% |
UINT16 |
3–15 (step 1) |
3 |
Y |
Current protection |
|
0x109B (4252) |
84 : 04 : 02 |
RW |
1 |
% |
UINT16 |
3–15 (step 1) |
3 |
Y |
Voltage protection |
|
0x109C (4253) |
84 : 04 : 03 |
RW |
1 |
% |
UINT16 |
1–15 (step 1) |
3 |
Y |
Frequency protection |
|
0x109D (4254) |
84 : 04 : 04 |
RW |
1 |
% |
UINT16 |
3–15 (step 1) |
3 |
Y |
Power protection |
|
0x109E (4255) |
84 : 04 : 05 |
RW |
1 |
mA |
UINT16 |
1–3 |
1 |
Y |
Analog input protection |
|
0x109F (4256) |
84 : 04 : 06 |
RW |
1 |
°C |
UINT16 |
2–15 |
5 |
Y |
Temperature protection |