DOCA0258EN-00

IP Allow List Page Body

IP Allow List Section

On the IP Allow List section, proceed as follows.

  1. Use the toggle key to turn the IP Allow List on or off.

  2. Confirm with APPLY.

Global IP Address/Range Section

On the Global IP Address/Range section, proceed as follows.

  1. Add or remove the global IP address in the IP Address/IP Range field.

  2. Select the appropriate access rights in the Access Rights field.

  3. Confirm with APPLY.

IP Address/Range Section

On the IP Address/Range section, proceed as follows.

  1. Use Add New option to add the IP address.

  2. Confirm with APPLY.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?