Analog Comparator Output Status
The table lists the analog comparator output status for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
RW |
Type |
Svd |
Description |
|---|---|---|---|---|
|
0x00C0 (193) |
R |
BOOL | N |
Analog comparator output 1 |
|
0x00C1 (194) |
R |
BOOL | N |
Analog comparator output 2 |
|
0x00C2 (195) |
R |
BOOL | N |
Analog comparator output 3 |
|
0x00C3 (196) |
R |
BOOL | N |
Analog comparator output 4 |
|
0x00C4–0x00CF (197–208) |
– |
– |
– |
Reserved |