DOCA0258EN-00

HTTPS

The table lists the HTTPS for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X Unit

Type

Range Default value

Svd

Description

0x1373 (4980)

85 : 01 : 69

RW

1

N/A

UINT16

0–0
(step 1)

0

Y

Reserved

0x1372 (4981)

85 : 01 : 6A

RW

1

N/A

UINT16

0–65535
(step 1)

443

Y

Port number

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?