DOCA0258EN-00

DPWS

The table lists the DPWS for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X Unit

Type

Range Default value

Svd

Description

0x1375 (4982)

88 : 01 : 6B

RW

N/A

N/A

UINT16

0: Disable

1: Enable

0

Y

Enable/disable

0x1376 (4983)

88 : 01 : 6C

RW

1

N/A

UINT16

0: Silent

1: Non Silent

0

Y

Silent Mode

0x1377 (4984)

88 : 01 : 6D

RW

1

N/A

UINT16

*

5357

Y

Port

foot note : port no
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?