DOCA0258EN-00

Inhibit Status

The table lists the inhibit status for the Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

RW

Type

Svd

Description

0x0240 (577)

R

BOOL N

No voltage inhibit

0x0241 (578)

R

BOOL N

Under voltage inhibit

0x0242 (579)

R

BOOL N

Trip inhibit

0x0243 (580)

R

BOOL N

Thermal inhibit

0x0244 (581)

R

BOOL N

Max starts inhibit

0x0245 (582)

R

BOOL N

Interlock 1 inhibit

0x0246 (583)

R

BOOL N

Interlock 2 inhibit

0x0247 (584)

R

BOOL N

Interlock 3 inhibit

0x0248 (585)

R

BOOL N

Interlock 4 inhibit

0x0249 (586)

R

BOOL N

Interlock 5 inhibit

0x024A (587)

R

BOOL N

Interlock 6 inhibit

0x024B (588)

R

BOOL N

Interlock 7 inhibit

0x024C (589)

R

BOOL N

Interlock 8 inhibit

0x024D (590)

R

BOOL N

Interlock 9 inhibit

0x024E (591)

R

BOOL N

Interlock 10 inhibit

0x024F (592)

R

BOOL N

Interlock 11 inhibit

0x0250 (593)

R

BOOL N

Interlock 12 inhibit

0x0251 (594)

R

BOOL N

Local DI stop inhibit

0x0252 (595)

R

BOOL N

Remote DI stop inhibit

0x0253 (596)

R

BOOL N

Communication stop inhibit

0x0254 (597)

R

BOOL N

Force stop inhibit

0x0255 (598)

R

BOOL N

Antibackspin inhibit

0x0256 (599)

Reserved

0x0257 (600)

R

BOOL N

Direction change inhibit

0x0258 (601)

R

BOOL N

Speed change inhibit

0x0259 (602)

R

BOOL N

Custom stop inhibit

0x025A (603)

R

BOOL N

Firmware update inhibit

0x025B–0x025F (604–608)

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?