DOCA0258EN-00

Analog Module Data

The table lists the analog module data for Modbus TCP/IP and EtherNet/IP communication.

Modbus TCP/IP Address (Register)

EtherNet/IP Address

RW

X

Unit

Type

Svd

Description

0x15D1 (5586)

72 : 04 : 01

R

0.1

mA

INT16

N

Analog input 1

0x15D2 (5587)

72 : 04 : 02

R

0.1

mA

INT16

N

Analog input 2

0x15D3 (5588)

72 : 04 : 03

R

0.1

mA

INT16

N

Analog input 3

0x15D4 (5589)

72 : 04 : 04

R

0.1

mA

INT16

N

Analog input 4

0x15D5–0x15D8 (5590–5593)

72 : 04 : 05 – 72 : 04 : 08

Reserved

0x15D9 (5594)

72 : 04 : 09

R

0.1

mA

INT16

N

Analog output 1

0x15DA (5595)

72 : 04 : 0A

R

0.1

mA

INT16

N

Analog output 2

0x15DB–0x15DC (5596–5597)

72 : 04 : 0B – 72 : 04 : 0C

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?