DOCA0258EN-00

Ethernet Page Body

The Ethernet page contains the following sub-menus:

Level 1 Level 2 Parameter Name
Ethernet Global Statistics* Frames Received OK Frames Received
Frames Transmitted OK Frames Transmitted
Reception Errors Reception Errors
Transmission Errors Transmission Errors
Ethernet Port 1 Statistics Link Speed Link Speed
Duplex Mode Duplex Mode
Ethernet Port 2 Statistics Link Speed Link Speed
Duplex Mode Duplex Mode
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?