DOCA0258EN-00

Modbus TCP Port Diagnostics

The table lists the Modbus TCP global diagnostics for the Modbus TCP/IP communication.

Modbus TCP/IP Address (Register)

RW

X Unit Range Default value

Svd

Description

0xA80A (43019)

R

1

0–4294967295

Connection 1 Remote IP

0xA80C (43021)

R

1

0–65536

Connection 1 Remote port

0xA80D (43022)

R

1

0–65535

Connection 1 Local Port

0xA80E (43023)

R

1

0–4294967295

Connection 1 Received Messages

0xA810 (43025)

R

1

0–4294967295

Connection 1 Transmitted Messages

0xA812 (43027)

R

1

0–4294967295

Connection 1 Sent Errors

0xA814 (43029)

R

1

0–4294967295

Connection 2 Remote IP

0xA816 (43031)

R

1

0–65536

Connection 2 Remote port

0xA817 (43032)

R

1

0–65535

Connection 2 Local Port

0xA818 (43033)

R

1

0–4294967295

Connection 2 Received Messages

0xA81A (43035)

R

1

0–4294967295

Connection 2 Transmitted Messages

0xA81C (43037)

R

1

0–4294967295

Connection 2 Sent Errors

0xA81E (43039)

R

1

0–4294967295

Connection 3 Remote IP

0xA820 (43041)

R

1

0–65536

Connection 3 Remote port

0xA821 (43042)

R

1

0–65535

Connection 3 Local Port

0xA822 (43043)

R

1

0–4294967295

Connection 3 Received Messages

0xA824 (43045)

R

1

0–4294967295

Connection 3 Transmitted Messages

0xA826 (43047)

R

1

0–4294967295

Connection 3 Sent Errors

0xA828 (43049)

R

1

0–4294967295

Connection 4 Remote IP

0xA82A (43051)

R

1

0–65536

Connection 4 Remote port

0xA82B (43052)

R

1

0–65535

Connection 4 Local Port

0xA82C (43053)

R

1

0–4294967295

Connection 4 Received Messages

0xA82E (43055)

R

1

0–4294967295

Connection 4 Transmitted Messages

0xA830 (43057)

R

1

0–4294967295

Connection 4 Sent Errors

0xA832 (43059)

R

1

0–4294967295

Connection 5 Remote IP

0xA834 (43061)

R

1

0–65536

Connection 5 Remote port

0xA835 (43062)

R

1

0–65535

Connection 5 Local Port

0xA836 (43063)

R

1

0–4294967295

Connection 5 Received Messages

0xA838 (43065)

R

1

0–4294967295

Connection 5 Transmitted Messages

0xA83A (43067)

R

1

0–4294967295

Connection 5 Sent Errors

0xA83C (43069)

R

1

0–4294967295

Connection 6 Remote IP

0xA83E (43071)

R

1

0–65536

Connection 6 Remote port

0xA83F (43072)

R

1

0–65535

Connection 6 Local Port

0xA840 (43073)

R

1

0–4294967295

Connection 6 Received Messages

0xA842 (43075)

R

1

0–4294967295

Connection 6 Transmitted Messages

0xA844 (43077)

R

1

0–4294967295

Connection 6 Sent Errors

0xA846 (43079)

R

1

0–4294967295

Connection 7 Remote IP

0xA848 (43081)

R

1

0–65536

Connection 7 Remote port

0xA849 (43082)

R

1

0–65535

Connection 7 Local Port

0xA84A (43083)

R

1

0–4294967295

Connection 7 Received Messages

0xA84C (43085)

R

1

0–4294967295

Connection 7 Transmitted Messages

0xA84E (43087)

R

1

0–4294967295

Connection 7 Sent Errors

0xA850 (43089)

R

1

0–4294967295

Connection 8 Remote IP

0xA852 (43091)

R

1

0–65536

Connection 8 Remote port

0xA853 (43092)

R

1

0–65535

Connection 8 Local Port

0xA854 (43093)

R

1

0–4294967295

Connection 8 Received Messages

0xA856 (43095)

R

1

0–4294967295

Connection 8 Transmitted Messages

0xA858 (43097)

R

1

0–4294967295

Connection 8 Sent Errors

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?